WIKA Singapore

Glass level gauges

Individual design and corrosion-resistant materials

Continuous and direct level indication without supply voltage: glass level gauges from WIKA consist of a gauge body that constitutes the main element. A liquid channel is machined into it. Other elements are valve heads, process connections, glasses and/or mica shields. The use of mica shields is recommended for certain applications and high temperatures.

FAQ
FAQ

How long is the WIKA Build ID valid?

The WIKA Build ID is valid for at least three months.

How does a reflex sight glass level indicator work?

The principle of the reflex level indicator is based on the reflection of light. In the gas or steam phase, the light is reflected by the prismatic grooves of the sight glass so that bright indication is achieved. In the liquid phase, the light is ...

more