WIKA

Multipoint thermometers

WIKA multipoint thermometers: worldwide leaders in temperature measurement

Multipoint thermometers are used in various applications in the refining and petrochemical industry. WIKA is a world leader in flexible multipoint sensor thermometry and the preferred solution of many major companies and licensors. Our preferred advanced multipoint solutions, including FLEX-R® and FLEX-O®, are recognised as leading technologies in the industry. Additional multipoint products for global market requirements include traditional multipoint designs such as pipewells, T-bar, spring-loaded, bimetallic spring, and heat transfer block. Innovative mini-multipoint solutions where point density and thermocouple size matter include both stuffed and drawn assemblies to solve challenging applications.

FAQ
FAQ

Can the FLEX-R® be installed in the reactor in the horizontal position?

Yes, the FLEX-R® can be installed in any position. However, care should be taken to ensure the internal structures are tightly secured in their proper position.

Does WIKA offer installation assistance?

Yes, we offer full service installation when there is a critical need to meet a fast schedule for installation. We can supply the personnel necessary to route, position, test and commission our assemblies. Alternatively, WIKA can also supply superv ...

more

What is a secondary containment chamber?

The secondary containment chamber is a sealed chamber (neck tube) between the primary seal weld and secondary seal weld that contains an instrument connection. In the event of a primary weld failure, the secondary containment chamber would pressure ...

more