WIKA

Unit calculator






Note
The conversion function made available here has been created with the utmost care. However, we exclude any liability for the correctness of the result.

General information

Pressure Units

Pressure as a measurement parameter

In the field of pressure measurement technology, there are many other units besides bar and psi. You can use the unit converter to convert, for example, mbar to μbar, Pa to kPa or mmWs to mWs.

Further common units for the measurand pressure:

  • MPa
  • kp/mm2
  • atm
  • inH2O
  • mmHg (Torr)
  • kp/cm2 (kg/cm2)
  • ftH2O
  • inHg

If you want to convert the two most common units, bar and psi, you'll need the exact conversion values. If you want to convert bar to psi, multiply the bar value by 14.503774. In the opposite direction, a psi value is multiplied 0.068948 in order to determine the unit in bar.

  • 1 bar = 14.503774 psi
  • 1 psi = 0.068948 bar
Beispiel Tabelle
Einheit Unit bar mbar Pa N/ m2 kPa kN/m2 MPa MN/m2 atm mmWS Torr mmHg psi
1 bar 1 1000 10⁵ 100 0.1 0.986923 1.019716*10⁴ 750.0638 14.503774
1 mbar 0.001 1 100 0.1 10⁻⁴ 0.966923*10⁻³ 10.19716 0.7500638 0.014503774
1 Pa 1 N/m² 10⁻⁵ 0.01 1 0.001 10⁻⁶ 0.986923*10⁻⁵ 0.1019716 0.007500638 1.4503774*10⁻⁴
1 kPa 1 kN/m² 0.01 10 1000 1 0.001 9.86923*10⁻³ 101.9716 1.500538 0.14503774
1 MPa 1 MN/m² 10 10⁴ 10⁶ 1000 1 9.86923 1.019716*10⁵ 7500.628 145.03774
1 atm 1.01325 1013.25 101325*10⁵ 101.325 0.101325 1 1.033227*10⁴ 160.0021 14.695949
1 mmWS 9.80665*10⁻⁵ 0.0980665 9.80665 980665*10⁻³ 9.80665*10⁻⁶ 9.67841*10⁻⁵ 1 0.073556 1.422334*10⁻³
1 Torr 1 mmHg 1.33322*10⁻³ 1.33322 133.322 0.133322 0.133322*10⁻³ 1.315789*10⁻³ 13.59506 1 1.933672*10⁻²
1 psi 6.89476*10⁻² 68.9476 6894.76 6.89476 6.89476*10⁻³ 0.068046 703.06958 51.715075 1

Temperature Units

Temperature as a measurement parameter

In the field of temperature measurement technology, the units are differentiated in accordance with the international system of units, SI for short. The temperature is measured in degrees Celsius (°C) or in kelvin (K). The measurement of temperature in degrees Fahrenheit (°F) is mainly used in the USA or occasionally in United Kingdom. The unit kelvin, on the other hand, is mainly used in science.

Units for the measurand temperature:

  • Degrees Celsius (°C)
  • Degrees Fahrenheit (°F)
  • Kelvin (K)
  • Degrees Rankine (°Ra or shortened °R)

Conversion table and conversion factors for the most common temperature units

If you should want to convert Celsius to kelvin, you have to add 273 to the Celsius value. When converting from Celsius to Fahrenheit, on the other hand, the Celsius value is first multiplied by 1.8 and then 32 is added to the result.

With the WIKA unit converter, you can, for example, convert Celsius to Fahrenheit, kelvin to Celsius or Fahrenheit to Rankine when dealing with temperatures.

Temperatureinheiten_DE
HTML-Tabelle
°C Celsius °F Fahrenheit K Kelvin ° R Rankine
Boiling water 100 °C 212 °F 373.15 K 671.67 °Ra
Human Body 37 °C 98.6 °F 310.15 K 558.27 °Ra
Room temperature 21 °C 69.8 °F 294.15 K 529.47 °Ra
Freezing point of water 0 °C 32 °F 273.15 K 291.67 °Ra
Absolute Zero -273.15 °C -459.67 °F 0 K 0 °Ra